Wave Winding
An armature winding in which two coils are connected in series and follow each other on the surface of the armature like waves such that there are only two paths for the current flow irrespective of the number of poles In the circuit.
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
An armature winding in which two coils are connected in series and follow each other on the surface of the armature like waves such that there are only two paths for the current flow irrespective of the number of poles In the circuit.