Main Lobe
Main lobe is the lobe of the radiation pattern of a directional antenna which contains the direction of maximum radiation. This is the lobe that exhibits the greatest field strength. It is also called as main beam.
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
Main lobe is the lobe of the radiation pattern of a directional antenna which contains the direction of maximum radiation. This is the lobe that exhibits the greatest field strength. It is also called as main beam.